Part Number: LSF0102-Q1
Other Parts Discussed in Thread: TXU0202, TXS0102
Hi There,
For below mentioned configuration of LSF0102-Q1, IC is consuming ~25uA current during sleep mode. During sleep mode:
- 3.3V_BLE = 0V, 5V_MCU = 5V will be available.
- B1 & B2 are pulled up with 1k.
I need to put IOs in tristate mode during sleep mode. What can be the best possible way ?
- Can I connect OE w.r.t Vref_A=3.3V_BLE. Since It is not available during sleep so OE will not trigger internal FETs ?
- Do I need to drive OE from MCU I/O tolerant to 5V ? Is it allowed ? In that case whether OE still needs to be shorted with Vref_B ?