Part Number: ADC128S102QML-SP
Other Parts Discussed in Thread: ADC128S102
Hi, I've had issues with the ADC128S102 breaking. The power sequence is correct for power on. Do I need to be concerned with power off? Can i continuously have the system apply voltage to the inputs and have current entering the part if it's <10mA per pin and <20mA total if the part's VD and VA rails are off?