TPS65982: TPS65982 USB3.0 only application

Part Number: TPS65982
Other Parts Discussed in Thread: TUSB1146,

I'm using the TPS65982 in combination with the TUSB1146. With my configuration, 2-lanes DP/USB3.0 and 4-lanes DP work. When I try to use USB3.0 only, I can see that my USB3_event doesn't trigger. I want this to work correct. Is there any way to fix this problem?

usb3.0 only:                 DP mode event = 0V        USB3 event = 0V

2-lanes dp/usb3.0:      DP mode event = 3.3V        USB3 event = 3.3V

4-lanes dp :                 DP mode event = 3.3V        USB3 event = 0V

image.png