This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5296A: ADS5296A - VCM issue

Part Number: ADS5296A

Hi,

 

The ADC is power up after the diff op amp.  VCM open in the diff op amp cause the output to be in the mid scall which is greater the the ADC input ABSOLUTE MAXIMUM RATINGS. To eliminate this I want to put Pull Down resistor (3.3K -> ~300 uA when VCM is 0.9V) on the VCM.

    is it acceptable?

    pls. advise

 

regards

zeev gerber