Part Number: ADS9817
Hi team,
I am currently designing a system using the ADS9817, but I am experiencing an issue where the AD conversion results exhibit minor fluctuations and lack stability.
Circuit Configuration:
- Analog Inputs (AIN1 to AIN8): All negative (M) terminals are tied to GND.
- Positive Inputs (P): Connected to the outputs of 8 individual differential amplifiers.
- Test Condition: For experimental purposes, the +/- inputs of the differential amplifiers are shorted together. Therefore, the output voltage from the differential amplifiers is 0V.
Symptoms:
When plotting the AD conversion data under this condition, we observe minor fluctuations in the output.
What puzzles us is the behavior over time, temperature, and during re-initialization:
When plotting the AD conversion data under this condition, we observe minor fluctuations in the output.
What puzzles us is the behavior over time, temperature, and during re-initialization:
- Behavior after Power-On:
Immediately after turning on the power, there is almost no fluctuation in the AD results. However, when taking measurements a few minutes later, the fluctuations appear. The peak-to-peak amplitude worsens by a factor of approximately 10, and the data plots for all 8 channels overlap perfectly. Furthermore, the cycle of these fluctuations appears to be close to the power supply noise line frequency. - Cooling Test Results:
To check for thermal effects, we used a spot cooler to cool down the ADS9817 while it was in the fluctuating state and took measurements immediately after. However, the fluctuations remained unchanged, suggesting that the issue is not caused by IC temperature rise. - Behavior after Re-initialization:
While keeping the power on, if we execute the initial configuration settings for the ADS9817, the fluctuations immediately disappear. However, after leaving it for a few minutes, the fluctuations return when we measure again.
Re-initializing the device seems to temporarily stabilize the operation. Could you please advise on what might be causing this behavior?
Thank you for your support.