AFE7900EVM: AFE7900EVM: Only Channel A configurable via Latte Scripts, other channels unresponsive

Part Number: AFE7900EVM

Hi,

I'm using the Latte Scripts to configure the AFE7900EVM, and I'm running into an issue where only Channel A responds to configuration — the remaining channels (B, C, D, etc.) do not appear to be configurable / do not reflect the settings I apply.

Setup details:

  • Latte GUIversion: 2.9.0
  • Clocking setup (external LO/reference source, if any): External (1474.56MHz)

Attached: Latte Scripts

Any guidance on what might cause only one channel to respond — e.g., an SPI addressing/chip-select issue, a script config flag, or a channel-enable register I might be missing — would be appreciated.

latte_scripts.zip