Part Number: ADC32RF54
Other Parts Discussed in Thread: TMP102
Hello Experts,
I am currently designing a system using the ADC32RF54, and I understand that the device does not include an internal temperature sensor.
What would be the recommended method to estimate or monitor the internal junction temperature (Tj) with reasonable accuracy?
I am considering using a TMP102 placed close to the ADC32RF54 pad to estimate its temperature. However, I am concerned that the measured temperature may differ significantly from the actual junction temperature.
I also considered estimating the junction temperature based on the power-rail currents, but this would require monitoring multiple power rails, and I would prefer to avoid adding several current-monitoring ICs.
If I use a TMP102 to monitor the temperature near the ADC32RF54 package, what temperature margin would you recommend applying to ensure that the ADC32RF54 junction temperature remains safely below its maximum rating?
Best regards,
Filipe