DAC11001B: THD TEST DATA

Part Number: DAC11001B

 

Hello,

I am currently evaluating the DAC11001B and reaching out with an inquiry, as the measured THD performance does not match the specifications listed in the datasheet.

Currently, I am getting a THD measurement of approximately 0.0009%, whereas the datasheet (PDF) indicates around 0.000398% under the same conditions.

Despite using identical test conditions—a filter range of 22Hz to AES17 (40kHz), a 192kHz sample rate, and a 1kHz tone frequency—there is a significant discrepancy in the values, which I am trying to understand. I also observed the same results at the buffer stage following the DAC.

Could you please help clarify this issue?




Ti_DAC11001A_audio.pdf