Part Number: ADS124S08EVM
I am running the predefined Current Measurement script on the ADS124S08EVM board. 5 mV is appplied across the current shunt resistor R78. The mean reading on the Time Domain tab in the Analysis Engine is 15197 with PGA gain of 1. With no input to J9 pins 2 and 3 (across R78) the mean offset is 127. If the gain is changed to 2, the mean reading is 20612. I expected something closer to two times 15197 or 30394. Likewise with PGA gain of 4 I get 24170 and I expect 60788. What am i not understanding?