Part Number: ADCS7476
The datasheet for ADCS7476AIMF/NOPB has an "Absolute Maximum Ratings" table on the tob of page 4 showing that the Maximum "Soldering temperature, infrared (10 sec) " is 215°C, but the "packaging information" table on page 28 shows a max reflow temp of 260°C. Can you please confirm the correct max reflow temp and time?