According to the datasheet of ADC12D1800, In DESIQ mode, the input bandwidth is 1.75GHz, However, the bandwidth is 2.7GHz in DESCLKIQ mode!
How should I connect the input signals? Could I connect the input signals in DESCLKIQ mode as DESIQ mode? Should I use the balun or power splitter to generate two exact same signals for VinI and VinQ?
Is there any requirements to the input signals in DESCLKIQ mode?