Other Parts Discussed in Thread: ADS7951, ADCPRO
Hi,
I started to utilize the TI ADS7951 and I see that when using a fast sampling rate, the reading are not accurate.
I am trying to test it on the EVB you provide me but get this error:
"Unable to locate the LabVIEW Run-Time engine. adcpro requires a version 8.5.1 (or compatible) Lab-VIEW Run-Time Engine. Please contact the vendor of ADCpro to correct this problem"
It looks like it supports only Win XP. I tried it on Win XP now and it doesn't work… it once recognized it and now the PC doesn't see it at all.
When I work in sampling rate of 1sps, it looks good. Once I raise the sampling rate to 100K I see that the measurement is not accurate.
Instead of 1000mV, I get 1020mV, and instead of 4V, I get ~3980mV. the reference voltage is 2.5V and only when I measure 2500mV, I get exactly 2500mV.
I looked with scope on the input and I see while sampling, a ripple of ~10-20mV of Sawtooh at the sampling rate frequency…
What could that be?
BR,
Rotem.