Dear sir:
I got some problem using DAC7728.
We are working on bipolar straight binary mode with hardwire strapping of RSTSEL=0, /USB=0. There should be a -Full-Scale value observed at the output. But we got 0V output. We tried to read back the DAC offset register but we got solid "000", not "99Ah" in page 39. We want the DAC output to be -Full-Scale at power up stage.
Thank you!
Brian