Hi,
Can I keep TESTN_PACE_OUT1 and TESTN_PACE_OUT2 pins floating when we I use softtware pace detection approach?
Thanks,
Sachin Nalbalwar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can I keep TESTN_PACE_OUT1 and TESTN_PACE_OUT2 pins floating when we I use softtware pace detection approach?
Thanks,
Sachin Nalbalwar
Hi Sachin,
If the PACE out pins are not used, they can be pulled high through weak pull up resistors. You will not want to keep them floating. You then can use one of the higher data rates within the ADS1298 to monitor to see if pacemaker signals are present.
Regards,
Tony Calabria
Hello Tony,
Thanks for the quick response.
As per ADS1298 datasheet,i can use only 8kSPS max, if i increase the data rate then ADC resolution will come down.
Regards,
SAchin Nalbalwar