I have the DAC1220EVM and have it operarting quite nicely, however, the output amp rolls over when approaching max output. This is a property of the op-amp, as monitoring the DAC output directly, things go to nearly the rails. Can you suggest a more modern op-amp that will not roll over and be single supply?
Next, I wish to use 2 ea DAC1220's in the system I am designing and wondder about using a single crystal. It seems a shame to have two crystals.
Also, since the system has 2 devices each will have its own CS\. Can I CS\ both devices for simultaneous RESET?
Can I CS\ both devices for the simultaneous CAL procedure if I use a dead wait time? Can I poll only one device to determiine if they have both completed CAL?
Thank you,
Tom Burdick