Hello,
I have an ADS1298ECG-FE board that we are using to run the software provided with the ECG Implementation on the TMS320C5515 DSP Medical Development Kit (MDK) with the ADS1298 ECG-FE and everything works fine.
Our target is to use the ADS1198 and ADS1194 (16 bit versions of the ECG FE) instead of the ADS1298 (24 Bits).
Is there any information on which changes in the sofware provided with the TMS320CD5515 DSP MDK are necessary so that we can test these 2 other 16 bit
versions of this ECG FE chip?
We already ordered the ADS1198ECG-FE board that came with the ADS1198ECGFE-PDK Front End Performance Demonstration Kit.
I know that I have to change the software to handle 16 bits (ADS1198) instead of 24 bits (ADS1298) but I can't get it to work correclty when I change the FE boards.
Thank you.
Eduardo