I need some help finding an Op Amp to drive the ADC14155QML-SP. The op Amp must receive a single-ended signal and provide differential outputs with a Vcm of 1.5V to be compatible with the ADC14155QML-SP. The single-ended input signal to the Op Amp is a log video signal so I need to use a DC coupled interface so i don't distort rise times of the pulses. Lastly, it needs to be a QML component for this application.
Thanks,