This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1282

When I switch input, DRDY pulses come in 63 ms after RDATAC command, as if after SYNC or calibration. Is it correct behavior? There is nothing written in datasheet about it.

  • Hi Sergey,

    Welcome to the forum!

    Yes, switching the channels in the multiplexer will reset the modulator.  After a register write operation, the ADC resets, resulting in an interruption of 63 readings.  If you are running at 1kSPS, this would account for the 63ms delay. 

    There is a note about this on the register write operation on page 36.

    Thank you and Best Regards,

    Luis