Other Parts Discussed in Thread: DAC7578
Hi, I'm creating a design around the DAC7578 QFN-24 package, using it to supply low-current voltages between 0-+5V, and had some questions I couldn't answer with the data sheet.
I'm more or less uninterested in using the CLR pin, can I let it float? Or do I need to connect it to +5V to prevent unwanted hardware resets?
Can I supply both AVdd and Vref with the same regulated +5V rail? What is the behavior if Vref and AVdd aren't supplied at the same voltage?
I'd appreciate any info. Thanks!