What is the latency from writing to SETUP register (bit3) to enable or disable the burnout current sources and the connection/disconnection of the sources to the ADC +/- inputs?
Is the PGA gain effected when the burnout currents sources (bit 3 of SETUP register) are enabled or disable if the same GAIN value is not changed (bit 2-0 are not changed)?