Other Parts Discussed in Thread: ADS7828
I'm using the ADS7828 in a new design where there may be voltage present on the analog inputs before the device is powered.
The voltage on the inputs will have a high source impedance and will not exceed the measurement range of the device, but it could be in this state for upto one second before the chip is fully powered up.
Whilst the Abs max section of the datasheet doesn't lists a spec for the analog inputs, the electrical characteristics section has a line for "Analog input: Absolute input range" being between -0.2 and +Vdd+0.2V. This implies that it's not okay to exceed the supply rail, but is it okay to do this for a short time as long as the current into the (presumably shottky-clamped) pin is less than a certain amount?
Thanks
James.