Other Parts Discussed in Thread: DAC8564, DAC8568
I use the Dac 8564 in two products.
Recently , i have discovered two issues ? , which i think are related somehow.
The problem
The dac, sometimes refuses to acknowledge spi commands and acts as if it is not selected. ( this may have been fixed by changing decoupling cap to 10uf from 1uf)
this happens when the device is cold but seems to stop misbehving when warmer, although i am hoping that the above 10uf cap will be the fix for this.
the more serious issue
The dac ref changes from 2.5V to a different voltage i.e 3.8V, 4.1V even though no parts are connected except for 1uf cap
This happens whenever a ramp or 100 % Fs SQ wave is generated by a SW test
This does not happen when zeros are loaded or a small amplitude sq wave is loaded ( 1/4 to 3/4 scale @1Khz, 20ksample/sec update)
When the int ref is set to "off" the ref pin goes to zero
Pwr is AVdd=5V from buffered ref, Vddio=3.3V pin 5,6 connected to Agnd
Why does to ref generate these peculiar voltages ? ( This seems to be releated to glitches generated by large output signal transitions, as it doesnt happen when constant values are output) The dac seems to work better when a sine wave is output but the problem still happens
I have tried,
100uf caps on psu pins
any other suggestions ?
Regards
Nick