Other Parts Discussed in Thread: ADS5400
1) Do the adaptor boards (shown for Xilinx & Altera) both come with the EVM?
2) Are there any of the main Xilinx or Altera boards that these adaptors don't work with? Or are these specifically designed for one or two of each?
3) Is the source code available? I saw that a few have requested and received the source code. Will the end customer need to request via forums?