Other Parts Discussed in Thread: ADS8328, TL431
I HAVE CONFIGURED ADS8328 IN
1)MANUAL CHANNEL SELECTION . 2) TRIGGER SELECT - MANUAL.
I HAVE SELECTED ONLY CH0.
VREF TO ADC8328. IS 2.5V.
I AM GIVING ANALOG INPUT (0V TO 2.5V) THROUGH AGILENT MULTIFUNCTION METER.
AND OBSERVED THE FOLLOWING READINGS.
|
SR NO |
INPUT (V) |
ADC COUNT |
|
|
1 |
1.000 to 1.005 |
27651 |
steady |
|
2 |
1.006 |
27651 , 28163 |
fluctuat |
|
3 |
1.007 |
27651 , 28163 , 28419 |
fluctuat |
|
4 |
1.009 |
28419, 28163 , 28546 |
fluctuat |
|
5 |
1.1 to 1.119 |
30723 |
steady |
|
6 |
1.120 |
3072 , 331491 |
fluctuat |
|
7 |
1.138 to1.157 |
31747 |
steady |
|
8 |
1.158 |
31747 , 32515 |
fluctuat |
|
9 |
1.5 to 1.509 |
40963 |
steady |
|
10 |
1.510 |
40963 , 41987 |
fluctuat |
|
11 |
2.4 to 2.404 |
64515 |
steady |
|
12 |
2.405 |
64515 , 65535 |
fluctuat |
|
13 |
2.410 |
65535 |
steady |
It is observed that adc value is not changing for all analog input s it remain constant for some range as in reading numbers - 1 ,5 ,7 ,9 ,11. i.e. adc count is not changing for every step change in analog input.
frquently It is observed that when fluctuating difference between adc count is 64, 256, 512 like this . for same analog input .
please help me for get rid of fluctuations and above step response.