This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5158 interrupt

Other Parts Discussed in Thread: TVP5158

I want to use the interrupt of TVP5158.

 I have set:

 0xAD= 0|(1<<6) |(1<<7);

0xF4h is set to enable all interrupt.

But there is no interrupt is generated.( ps : I connect the INTREQ pin of TVP5158 with a GPIO pin of DSP).

I want to know:

1  "signal prsent detect interrupt" is generated one time for each frame,or onlly when the TVP5158 is power on.

2 What "weak signal" means? Does it mean there are some video lines is lost ?

3  When will "Video (HV) lock change interrupt" be  generated.  Does it mean there are some video channel is wrong?

4 What does "Macrovision change interrupt" mean?

Could you help me?