Other Parts Discussed in Thread: ADS1230, ADS1232
Hi,
I wrote program in C & using Keil compiler, the header file & schematis are attached for your reference. The program is working fine with some load cells but for some load cells it is giving high value of counts i.e. more than 500K at no load conditions, now if I put some load then counts increases & becomes 0 & increases while increasing load. I hope the method of offset calibration used is not correct. Please review the header file & let me know the right method or send me the sample code for offset calibration. I saw the different behaviour for different load cell when starts the weighing machine, some times there is a reading before zero comes, some time fast fluctuations in counts & that is not readable.
Please suggest the solution..
Regards,
Navin Rana