Hi,
I am having some problems analysing the data from ADS1298 ECGFE.
I have provided sine waves having an amplitude 200mV p-p and a frequency of 10Hz and have set my PGA gain settings to 6 for all the channels.
Now,giving this input to just the channel 1 and on 'unchecking' the input referred data box in the scope tab,I am getting,as expected,an output of 1.2Vp-p.
1.On analysing the FFT of my data,I find that in the range of 0-20 Hz,I am getting SNR(dBFS) of -3.51.Should'nt I be expecting a better SNR?Can you tell me whether it is as expected?
It also says that the fundamental dB is -109.06.Can you please let me know what exactly does the fundamental dB value indicate??
I am also not sure whether I am getting the correct THD(dBc) values.
2. When I used the device with an arb signal from the function generator with amplitude of 47.6mVp-p and 10 Hz frequency with PGA of 6 and again unchecking the input referred data box,I found,in the output waveform that my signal is attenuated.Since I'll be performing experiments with eeg signals,I would be working with very low amplitude signals which needs to be largely amplified.Can you guide me as to where might be the problem.
Thanking you
Regards,
Shobhit