I'm having some trouble with the AFE7225 in LVDS mode. Currently I have CLKINN/P hooked up to DAC_FCLKN/P which is running at 100 mhz. DAC_DCLKN/P is running at 300 mhz and data is clocked in 600 mbps. All the clock dividers are set to 1 in the configuration. After applying sync internally. All the FIFO error conditions soon register.
I found the following in slos711a interesting:
" The read pointer increments at the DAC_DCLKIN rate whereas the write pointer increments at the divided DAC_CLK rate."
This statement is worrisome. If it is true in LVDS mode then the FIFO can't work. Am I supposed to be turning on FIFO bypass or is that statement incorrect?
Thanks,
Jon Pry