Other Parts Discussed in Thread: ADS1230
Dear Sir,
I interfaced ADS1230 with 8051.Its working fine,for the load cells 10kg,20kg,50kg......100kg.When connecting these load cells the internal counts(initial ADC counts without load) of the ADC will remains in positive,so there is no problem to calibrate and also it shows the exact weight.
But if i connected some other high capacity load cells such as200kg,300kg...750kg the initial counts without load will remain below zero.So if i calibrated without considering these negative counts,it seems skipping the starting value until the counts reaches positive, during weighing an object.
So what step should i take to eliminate these problems.Please Help..
Expecting Your precious suggestions...
Thanking You..
Ajit Plakkat