Hi,
I am looking for the schematic for ADS7951
I got some for ADS7952 and ADS7953 but not for 7951 on the below
Is the same schematic used for series 795x ?
or someone please help me to get the schematic.
thanks for your help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gary,
There are 'Symbols and Footprints' on the ADS7951 product folder which might help you. http://www.ti.com/product/ADS7951#cadsymfoot
Also, if you look at page 11 of the ADS7951 data sheet, you should notice that the pin out of the 4/8 channel devices is compatible with the 12/16 channel devices. If you always align on pin 1, the 38 pin package just just extended the channel numbering down the left side of the chip and wrapped around to the right. You can also look at the EVM for the ADS7953, that PWB supports all devices in the ADS795x family.
Hi Tom,
I have got the datasheet of ADS7953-EVM you said,
and the schematic is what I need for my ADC, thats really help.
Thanks