This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP7002 for 800x600@60Hz LCD panel

Other Parts Discussed in Thread: TVP7002

 

Dear Sir,

We use a 800x600@60Hz VGA signal from a PC. Provide to TVP7002 to drive a 800x600 LCD panel.

Now TVP7002 output clock is correct 40MHz but output timing is not we want.

- I need to arrange output HS/VS/DE timing to meet LCD spec, if LCD's timing is:

Hfp = 40 pixel

Hpw= 128 pixel

Hbp= 80 pixel

Hactive=800 pixel

Vfp = 1 line

Vpw= 4 line

Vbp= 23 line

Vactive=600

1.What signal for TVP7002 output HS/VS/DE align with ? Is it Input HS/VS ? Setting it from AVID register 0x40~0x49 ?

2.How to set AVID register correctly ? Sorry that I'm really not very clearly understand how to set AVID register .

 

Many thanks a lot !