Hello,
I'd like to convert a range of +-0,5 V with my ADS124 with unipolar 3,3-0 V voltage reference and power. To avoid putting a negative input to the device I thougt to measure the 0-5V using the voltage reference in the ADS, so my true input comes in range 2,5-2V aprox.
I studied the PGA and the ADC and I find this problem: if I use the AINp to measure, should I use the voltage reference in the AINN sol the input to the ADC is +-0,5V? In other words... Can I try to measure a bipolar range in ADC although I put a unipolar voltage analog input at the ADS?
I attach an image with my current idea and an alternative (although I don't really like it)
Which config should I use?
Thanks in advance