Other Parts Discussed in Thread: ADS5400, ADS5463, ADS4149, ADS5474
Hi,
I am using the TSW1200EVM to capture the output of an 8 bit 400Msps converter. The inputs to TSW1200 board are provided using the 120pin samtech connector that include 16 LVDS pairs (8 bits) + ADC clock (p and m). I have configured the EVM in single channel SDR format and am using the MATLAB interface with the FPGA. Everything works fine upto 250Msps but as soon as I make the conversion rate > 250Msps, I start seeing a distorted output spectrum with the energy of the fundamental smeared in all the bins (incoherent output). This happens right at 250MHz and even a small increment in conversion rate (say 252Msps) causes this problem. Is there a problem in the EVM configuration or the FPGA cannot take a clock input > 250MHz ? Please let me know what do you think about it.
Thanks
Vaibhav