Dear Sir,
I am designing a system where I want to measure the temperature and display the same on 7 segment using microcontroller. So I can easily make standalone temperature device but I want to produce 4-20ma also output corresponding to the temperature. I have selected XTR105 out of your products which will produce 4-20ma output. But this output will be used for data transmission. If I measure temperature using this 4-20ma output (putting 250 Ohm resistor) this will change my readings when actual load is connected to the 4-20ma output ( because the overall load resistance will change ).
Is there any solution using XTR105 or any other cheap product which can give temperature information as well as 4-20ma output ?
My preference will be PT100 sensor but any other thermocouple can also be connected.
Thanks and Regards:
Rakesh