Hi all,
We want to use a capacitive touch screen of size 3 - 4" for our project but this is the first time that we will use such a peripheral. We look both for touch panel and controller but cannot find satisfying information. Moreover there is not enough information about programming the controllers. As far as I understand there are some examples with MSP430 (as most of the time), but our DSP chip does not have such a software support or I couldn't manage to find it. The examples are MCU and controller specific which brings us to select our periheral as soon as possible to develop on it. We have EVM 5515 right now and first prototype will be developed over this evaluation module.
Any recommendation or stating point will be appreciated.
Regards.