Hi,
Could you please let me know below parameters of LMP90100?
1. ENOB (Non Free Resonation)
There is the table of ENOB( Non Free Resonation) In datasheet P.11.
Are these parameters Worst or Typcal ?
2.CMRR
There is the CMRR parameter in Datasheet P8 as the condition of 214.65SPS.
Could you please let me know CMRR at the condition of 20SPS? (min/ typ)
3.Comsumption Current at the condition of below parameters
-1ch of Single ended
-24bit ADC
-Gain= 100x (can I set 100x gain ? If I can't , please change 128x)
-20SPS
-VIN=10mV
-ENOB(Non Free Resolution) 17bit
-VA=VIO=3V or 5.5V
Thanks in advance for your help.
Best Regards,
Ryuji Asaka