Together with a DAC, I am using the ADS1112 in a fast closed measurement loop. I need to read from only 1 channel (Ain0) as fast as possible. What is the minimum delay I should set between I2C write to start conversion and I2C read ? The datasheet states 15samples/s in 16 bit ...is the conversion time 1/15s?
I plan to change to a faster converter ADS1115 which has 860samples/s rate....what is the min delay i should set? What is the conversion time for this converter?