This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About the analog input signal for ADS1271EVM-PDK

Other Parts Discussed in Thread: ADS1271

In "ADS1271EVM & ADS1271EVM-PDK User's Guide",it is said that "ADS1271 converters on board illustrate use of daisy-chain mode".If so, can I use these two A/D chips as a whole and input the analog signal by the J4.1(Auxiliary Signal Input 1 - Positive terminal, Pg 3) and J5.2(Auxiliary Signal Input 2 - Negative terminal, Pg 3)? Thanks

  • Hi Yixi,

    The ADS1271EVM provides 'daisy chain' capability by virtue of having two devices on the board.  These would be independent data converters though, you could not apply a differential signal between the two devices as if they were a single ADC.