Hello,
I gather from reading other posts that there is a plan to produce a stand alone replacement for the Data Converter Plug-in (DCP) which will be compatible with versions of CCS later than 3?
I am currently trying to compile and run the example code ADS1278-C6713-CCS3v1 (I got this code from another thread on this site)
I can compile and run it using CCS 3.1 and DCP 4.3 ok but no luck with CCS5 yet (using the ADS1278 header and code files produced using the DCP that were supplied in the project folder). DCP 4.3 doesn't seem to work with CCS5.
My questions for now are....
1) When do you think the sand alone data converter support tool compatible with CCS5 will be available?
2) Will it support DSK 6713 and ADS1278 EVM
3) Will it work with DSP/BIOS 5.41?
Thank you very much for your help,
Grant