This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compatibility of ADS5463EVM with DE2-115

Other Parts Discussed in Thread: ADS5463EVM, ADS58B19, ADS5517, ADS5474, HSMC-ADC-BRIDGE

Hi,

   I'm planning to use a DE2-115 to work with the ADS5463EVM, I have asked to Terasic about the speed of the HSMC and the say it can work at 640 MHz and that it can handle the requiered speed.

   There is other post asking about the compatibility of the DE2-115 with ADS5517, ADS5474 and ADS58B19 and it say that there is a family of EVM that could have some details.

   I would like to know if the ADS5463EVM is part of that family or it can work with an Altera HSMC with out problems.

Thanks,

Jose Jauregui

  • Hi,

    The HSMC-ADC-Bridge passive interconnect board enables the output of TI’s LVDS output high speed ADCs to be directly connected to a standard HSMC interconnect header, a typical input on the latest Altera FPGA EVMs. This enables users of TI’s high speed data converter EVMs to directly interface to Altera FPGA’s for prototyping purposes, saving the time and cost of producing a custom prototyping board. You can find the detailed info from the link below.

    http://www.ti.com/tool/hsmc-adc-bridge

    Thanks,

    KW