Hi,
I would like to ask two question for ADC14DC080 as below;
1,
In P3 and P14 of datasheet, it states that the differential full-scale input signal level is 2VP-P. But this ADC has 1.2V of internal VREF, then can we use 2.4VPP of input signal level? Or can we use input signal level by 2VPP if we will use 1.2V VREF?
2,
Could you please let us know the delay of DRDY output from CLK output? We could not find this information from datasheet.
Best Regards,