Other Parts Discussed in Thread: ADS1282
Dear Community
I currently used ads1282 adc in a project, according to the datasheet, the noise rms value should be around 1.1uV@1ksps by snr=20log10(Srms/Nrms), however, the tested result was about 30uV, i am not sure if there was something i missed.
the following is the test environment:
dvdd=3.3V
avdd=2.5V,avss=-2.5V
vrefp=2.5V,vrefn=-2.5V
bypass pin connected to a 1uF capitor
mclk=4.096MHz
1ksps, gain=1, mux=3'b010 - use internal resistors connected to (avdd+avss)/2 to test noise rms value.
the above picture is the noise wave in time domain.
Thanks for any answer.
ingdxdy