This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5662 sample rate

Other Parts Discussed in Thread: DAC5662

What is max sample rate of the DAC5662 using interleaved data input mode?

thanks.

  • Hi,

    DAC5662 datasheet specifies,

    In single-bus interleaved mode, the data should be presented interleaved at the I-channel input bus. The Q-channel input bus is not used in this mode. The I-channel input data rate is twice the update rate of the DAC core. As DAC5662 has 275 Msps of update rate, the channel-I input rate is max 550Msps but each of I/Q sample rate has to be max 275Msps.

    Thanks,

    KW