when i test RTD1 channel,i switch ADC to AIN6 and AIN7 ,activate IDAC1 and IDAC2, and then get the temprature which is about 30 degree.after that I connect the same pt100 to RTD2 channel, and then reset ads1148, switch ADC to AIN2 and AIN3,reactivate IDAC1 and IDAC2,but the temprature is about 32 degree.this is why?5707.SCHEMATIC1 _ 07-AIO.pdf