I noticed that the ADS1299 datasheet (SBAS499A) latest rev shows that pin 64 is reserved, and an output, and states that one should "Leave as open circuit". However, in the Evaluation Kit documentation (SLAU443, May 2012) schematic shows pin 64 tied to GND (pg 50)! Is there a mistake on the schematic? I can't see that an output should be tied to GND.
Also, are the design files &/or gerbers for the evaluation board available?