ADS1282 is configured successfully for 250SPS, 500SPS and 1000SPS.
When it is configured for 4000SPS it is automatically switched to 1000SPS.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADS1282 is configured successfully for 250SPS, 500SPS and 1000SPS.
When it is configured for 4000SPS it is automatically switched to 1000SPS.
Hello Sultan,
I need to ask you for a few more details. Are you using your own PCB board, or is this using the ADS1282EVM-PDK? How did you determine the data rate is not 4000SPS, are you monitoring the DRDY pin? If you are not using the ADS1282EVM-PDK; if possible, please provide the schematic and the SPI oscilloscope shots (DIN, DOUT, SCLK) when issuing the WREG command to change the data rate of the device.
Thank you and Best Regards,
Luis
Hi Sultan,
Have you resolved your issue with the sampling rate on the ADS1282?