Hi
I'm trying to download the patch code.
But, it seems that the patch is not downloaded properly.
[1]
I checked the updated version are 0x04 and 0x8C but DM365 can't get the image.
( The interrupt count for vpfe_capture0 in DM365 is not increasing. The image capturing is ok with version 4.00. )
[2]
In slea093.pdf, it says that i don't need to download the patch again by writing 0x05 to I2C address 0x10.
But, after HW reset or re-initializing driver for TVP5150, the version is back to 4.00 from 4.8C.
Is there any register to check whether the downloading is ok or not?
Even though the address 0x10 is set by 0x05, why the version goes back to 4.00?
Best Regards,
Jinkyu Park