Hi, I have a simple question about 8363.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I have a simple question about 8363.
Hi Alberto,
Special mode IV of the ADS8363 would let you run in Pseudo-differential mode using the sequencer. You would have to set bits [13:12] to 'one' and follow up with bits [11:8] with 01, 11 to select CHA1, CHB1, CHA3, CHB3. You could not sequence A1, A3, B1, B3 though. The control lines get a little trickier in this mode, so you would have to have independent control over both CONVST and RD. It may be simpler for you to leave the ADS8363 in fully diff mode and tie Vref to the (-) inputs, you could then apply your SE input 0-5V signal to the four (+) terminals.
Thanks Tom.
I think You are right, the simplest solution is to enable REFIO1 (or 2) at 2.5V and connect to all inverting inputs.
Regards
Alberto