The spec for LM96550 ultrasound pulsar lists a max current of 2A for an entire chip at 2% duty cycle. Say, the IC is driven at +/-50V and drives an ultrasound transducer, which is 50Ohm real resistance. The RMS of the output waveform is about 35V. Then the instantaneous current is 35/50=0.7A per channel. Is it possible to excite all 8 channels synchronously at these driving voltages and not damage the IC? Do I need to significantly lower down the voltages? How does the max current restriction changes with lower duty cycles?
Thanks.
Eugene