Hello all, I am using this part to sample a video signal where the sampling point is critical. The clkp input is AC coupled to an LVCMOS source (3v3) and clkm is AC coupled to VCM. The data sheet indicated the sampling point is the posotive edge of clkp however during extensive testing it became clear the device is sampling on the NEGATIVE edge of clkp.
Further strange behaviour wrt to data sheet is output data changes shortly after negative edge of clkp and the output clock is a short negative going pulse with its leading edge shortly after the data changes. I am running the device in low clock speed mode at 3.125Mhz, the input clock is continious, output data is LVCMOS and offset binary.
Any comments much apreciated!
Roger
I added this scope shot showing the input voltage, D14 output and adc clock to illustrate the problem (ignore ch4 its a trigger)